Loading...
Selected products added to your list. To view the list, Click here

GFCI Outlets & Receptacles

Advanced technology helps protect against electrical shock

Washing hands in bathroom sink
Electrical safety is a priority in every home. Leviton safety devices help protect people and property all while meeting or exceeding National Electric Code® (NEC®) standards. Our extensive line of SmartlockPro® Self-Test GFCI (Ground-Fault Circuit Interrupter) Receptacles includes: Standard, Weather-ResistantCombination GFCI/USBCombination GFCI/SwitchGuide LightAudible AlertSmart GFCI, Dual Function AFCI/GFCI and Blank Face. All of our GFCI receptacles and circuit breakers are engineered to help protect people from the hazards of electric shock and electrocution by interrupting power if a ground-fault is detected. GFCI outlets are required by the NEC® for areas around the home within a close proximity to a water source, such as kitchens, bathrooms, laundry rooms, basements, garages/carports and outdoor areas such as pools, spas, decks and patios.

Superior GFCI Protection. Advanced Technology. Only from Leviton.

Superior GFCI Protection
1
Leviton Patented Reset Lockout

Prevents reset if GFCI is damaged and cannot respond to a ground-fault

2
Terminals Withstand High Torque

Tolerates high-torque power tool installation and prevents wire pullout

3
Tamper-Resistant Shutters

Meets NEC® 406.12 requirement by blocking access to the contacts unless a two- or three-prong plug is inserted

4
Back and Side Wire

Two convenient wiring options; the external clamp also provides visual indication of proper wire seating

5
Status Indicator Light

Red and green LED indications provide simple, intuitive feedback on power and protection status as well as correct wiring

6
Standard Self-Ground Clip

Grounds the device in grounded metal box installations

7
Only 1.026” Protrusion into Wallbox

Takes up to 25% less space in the wallbox vs. other GFCIs for easier installation

8
Exceeds UL Safety Standards

Ground-fault and dual-function circuit breakers exceed UL safety standards.

9
Hydraulic-Magnetic Trip Technology

Hydraulic-magnetic trip technology ensures precise tripping even in extreme temperature ranges.

10
Easy-to-Read Diagnostics

Easy-to-read LEDs help communicate trip condition and type of fault.

11
Smart-Enabled Available

Optional Wi-Fi® or Ethernet connectivity with the My Leviton app.

Learn more »
Leviton’s patented reset/lockout feature on all of our SmartlockPro® GFCI receptacles prevent reset of the device if for any reason it is unable to respond to a ground-fault or if it is not wired correctly. Additionally, all of our GFCIs conduct an automatic self-test which improves safety by regularly confirming they can respond to a ground-fault. 

Where to Install

Kitchens
Install GFCI in Kitchens
Basements
Install GFCI in Basements
Bathrooms
Install GFCI in Bathrooms
Garages
Install GFCI in Garages
Laundry Rooms
Install GFCI in Laundry Rooms
Outdoor Areas
Install GFCI in Outdoor Areas

Slim Profile for Easier Installation

Leviton SmartlockPro® outlets feature the slimmest profile on the market for easy installation, every time.

Our GFCIs sit closer to the wallplate for a polished appearance.

Extra room for new construction and retrofit applications.

Only 1.026" protrusion into wallbox.

What are Ground-Faults?

  • Ground-faults occur when a current flows along an unintended path, such as through water or a person.
  • Since their invention in the 1970s, GFCIs have played an important role in helping to reduce the occurrence of shocks and electrocutions.
Mother and child brushing teeth in bathroom
Leviton's GFCI Circuit Breakers

How are Leviton GFCI Circuit Breakers Different?

  • GFCI and GFPE Circuit Breakers are available in standard or smart varieties which allow you to remotely monitor, update and trip your breaker from anywhere in the world with the MyLeviton app and feature the fastest installation on the market today.

Why Choose a Leviton GFCI?

  • Protection without exception. Other manufacturers may allow their GFCI devices to be reset even after protection is permanently lost – taking advantage of UL exemptions and providing users with unprotected power. Why take chances?
Child and his dog taking a bath

Videos

The Leviton GFCI Portfolio

Learn more about our variety of GFCI outlets to meet any application.

Leviton GFCIs on Today’s Homeowner

Learn more about our Self-Test GFCI outlets from Danny Lipford.

Leviton Answer Series: GFCI Line-Load Reversal

What to do if your GFCI is not working. Common wiring mistakes.

Leviton Answer Series: Preventing Electrical Shock

Learn how to keep your family safe from electrical shock with Leviton GFCIs.

Leviton Presents: How to Install AFCI/GFCI Outlets

Learn how to wire and install our AFCI/GFCI outlets.

The Easy to Install GFCI

See why Leviton is the clear choice for your next DIY installation.

Leviton Answer Series: What To Do When Your GFCI Trips

What you can do when your GFCI trips and when it’s time to call an electrician.

GFCIs (Ground-Fault Circuit Interrupters) Frequently Asked Questions

If your GFCI does not reset after installation this is often the result of reversing the LINE and LOAD wires when installing. You can diagnose this when you flip the breaker to reconnect power and the indicator light is green while the GFCI will not allow you to reset. This can easily be addressed by correcting the wiring. Take a look at the back of the device you are installing to note which side is the LINE and which side is the LOAD and attach the wires accordingly. Simply connecting the wires exactly the same as they are on the older device may cause this reversal. Leviton GFCIs protect against being reset unless they are properly wired, operating correctly, and connected to power.

The GFCI has internal parts that automatically conduct a test on regular intervals to ensure that the GFCI sensing and trip capabilities are intact. If the self-test sequence determines there is a potential loss of protection the GFCI will need to take specific actions such as tripping or providing an indication to alert end users.

The terms are interchangeable and mean the same thing. UL uses the term auto-monitoring and many of the GFCI manufacturers use the term self-test.

All the GFCIs manufactured after June 29, 2015 must include the auto-monitoring and many of the GFCI manufacturers use the term self-test.

No, as long as the outlet is not worn and you have conducted the manual test to ensure it is providing protected power. If you are doing a renovation or are looking to upgrade your older GFCIs, the self-test models do add an additional layer of protection.

Only the Leviton Audible GFCIs provide audible indication. All other wallbox mounted GFCIs provide visual indication only.

The only way to tell is to press the "test" button and then the "reset" button. If the GFCI blinks RED once it is a self-test model. If the LED turns immediately to GREEN, it is a non-self-test model.

Yes, you should manually test your GFCIs on a monthly basis.

If the Leviton self-test has conducted a self-test and everything has checked out OK the indicator light will be green. If the indicator light is either not on or red you should conduct a manual test immediately. You can always conduct a manual TEST and RESET sequence to confirm the GFCI is functioning properly.

How Can We Help?

Do you have questions about our GFCIs?

Contact Us Now