Loading...
Selected products added to your list. To view the list, Click here

USB Outlets

Fast, powerful and code-compliant

Keeping your smartphones, tablets and other electronic devices up and running is essential to staying connected to family, friends and business. Whether you have one device or many, we have a Leviton USB outlet that is right for you.

Innovative

  • With technology evolving daily, it’s important to choose a USB power outlet that can keep pace. Leviton USB In-Wall Chargers are engineered to incorporate the latest technology, including Type-C charging ports and Power Delivery.

 

Powerful

  • With the higher power needs of home office equipment such as tablets and laptop computers, a power supply that can keep up is essential. Leviton's line of Power Delivery enabled USB In-Wall Chargers deliver maximum power for faster charging.
  • With 60W and 30W options, our USB outlets with power delivery charge your devices faster than standard outlets alone. Plus, our entire line of USB wall outlets features a smart chip which recognizes and optimizes the charging requirements of the connected device. This ensures each device gets the power level it needs to charge fast and efficiently.

Safety

Leviton has been at the forefront of developing electrical products with your safety in mind for over a century and our outlets with USB ports are no exception.

  • Overcurrent protection helps protect the devices from receiving too much power which can damage them
  • Internal regulator prevents electronics from overheating
  • Outlets are Tamper-Resistant
  • No data transfer capability

Explore Our USB Wall Outlets / Chargers

USB with Power Delivery

USB without Power Delivery

Specialty USB

Also Available in Renu, Hospital Grade & Pop-Up Floor Box

Tips to Optimize Charging

Turn off the device

Avoid using your device while charging.

Disconnect when fully charged

Don't overcharge! Conserve the lifetime of your battery by disconnecting when fully charged.

Use a shorter cord

Cord length may affect the power & speed of the charge. Longer cord lengths may increase charging time.

Use the cable that came with the device

Use the charging cord that came with the device. Replacement cords should be OEM grade quality or a certified charging cable.

Cables That Work with Our Products

Leviton USB wall outlets are compatible with most widely used cables on the market today

USB Frequently Asked Questions

Leviton USB In-Wall Chargers have USB Ports and most models have 15 Amp or 20 Amp Tamper- Resistant Outlets. They are designed for adapter-free charging for two USB powered electronic devices at once, leaving the outlets free for additional power needs.

Device

USB Charger

Total Charging Power

Single Port Charging Power

T5636

3 Amps

60 Watts

60 Watts

T5635

6 Amps

30 Watts

30 Watts

T5633 / T5833

5.1 Amps

25+ Watts

15 Watts

T5632 / T5832

3.6 Amps

18 Watts

12 Watts

USB4P

4.2 Amps

24 Watts

12 Watts

Product number

Rating

T5636

15A-125V

T5635

15A-125V

T5633

15A-125V

T5632

15A-125V

T5833

20A-125V

T5832

20A-125V

Yes, all Leviton USB In-Wall Chargers are designed to fit in a standard single gang wallbox measuring at least 3” x 2” x 11⁄2”.

No. USB In-Wall Chargers install the same as a standard outlet and can replace an existing outlet.

No. USB In-Wall Chargers cannot be used for split power applications.

Leviton USB In-Wall Chargers can charge the latest tablets, smartphones, standard mobile phones, handheld gaming devices, e-readers, digital cameras, and many more USB-powered devices including but not limited to:

  • Apple® Devices
  • Samsung® Devices
  • Google® Phones
  • Tablets
  • Smart and Mobile Phones
  • Blackberry®, Android Phones
  • Windows® Phones
  • Nintendo Switch
  • Bluetooth® Headsets
  • Digital Cameras
  • KindleTM, e-readers
  • GPS
  • Laptops with Type-CTM power ports (MacBook Pro® 2016 or later)
  • Watches including: Garmin, Fitbit® and Apple

Yes, they can be installed side-by-side or with any other standard wiring device.

The electronic device will indicate that it is charging. In addition, Leviton USB In-Wall Chargers have a smart chip that recognizes the requirements of the electronic device connected and delivers the optimal level of charge.

Charging time depends on the electronic device battery, the cord used and the electronic device capability. The Leviton USB In-Wall Chargers are designed with a smart chip that recognizes your electronic device’s charging requirements and maximizes the current delivered throughout the charging process to ensure the most efficient charging time.

Yes. Leviton In-Wall Chargers can charge as many tablets as there are available USB ports.

No. These devices are for charging only; there are no data transfer capabilities.

If the Leviton self-test has conducted a self-test and everything has checked out OK the indicator light will be green. If the indicator light is either not on or red you should conduct a manual test immediately. You can always conduct a manual TEST and RESET sequence to confirm the GFCI is functioning properly.

Yes, they can be used in locations downstream from GFCIs to ensure the outlet is protected from ground-faults.

USB Type-C is the latest standard for charging. With its smaller connector head and symmetrical, reversible orientation, it fits easily into phones, tablets, laptops and more. Designed to work with all operating systems, Type-C can provide higher power for faster charging.

USB Type-C is backwards-compatible with older versions of USB A, but you will need an adapter that has a Type-C connector on one end and an older-style USB Type A port on the other end. You can then plug your older devices directly into a USB Type-C port. The device will charge like any other Type A in-wall charger.

Thunderbolt3 and USB Type-C (3.1 Gen2) share the same cable type and port. Type-C is the physical shape of the connector, USB 3.1 and Thunderbolt3 are features embedded in the connector.

USB 3.1 and USB Type-C are different. USB Type-C is the shape of the connector and USB 3.1 and Thunderbolt3 are embedded in it.

Power Delivery is a revolutionary charging technology that supplies a higher level of power than standard charging offers. It delivers faster charging to the latest PD-enabled devices and is the ideal solution for tablets, laptops and other devices that require more power for optimal charging.

Using a Dual Type-C with Power Delivery (PD) USB In-Wall Charger is the ideal way to be certain all devices are receiving the highest level of power they can accept for the fastest charge. As PD becomes the standard, installing a USB Charger with PD is the best way to ensure the fastest charging of future PD-enabled devices.

Refer to your device manufacturer specification sheet for this information.

There a few things that Leviton recommends to maximize the charging effectiveness of your device:

  1. If you do not use the device while it is charging, it will significantly shorten the charging time.
  2. Use the charging cord provided with the device.
  3. Cord length may affect the power and speed of the charge. Longer cord lengths may take longer to charge.
  4. Replacement cords should be OEM grade quality or approved by the device manufacturer.

Yes, Leviton USB In-Wall Chargers are designed to charge older devices and can also adapt to the changing requirements of newer technologies.

The Leviton 4-Port USB Charger has four Type A USB Ports designed to charge electronic devices such as tablets, phones, e-readers, etc. It does not have an outlet; it is only a USB charging device offering 4.2 Amps of power with the ability to charge up to 4 electronic devices at once.

Leviton USB In-Wall Chargers are cCSAus listed and meet all National Electrical Code®requirements for tamper-resistant outlets.

Yes, they are tested to meet the industry requirements to withstand over 10,000 insertions.

Yes, they are backed by a 2-year limited warranty.

Leviton USB In-Wall Chargers are available at Leviton distribution, retail partners, online retailers and on leviton.com.

No. For added safety, if a GFCI trip occurs, power is automatically denied to the charging ports to help protect connected devices, and charging will not resume until the GFCI has been reset.

How Can We Help?

Do you have questions about our USB Wall Outlets / Chargers?

Contact Us Now